Keysight License Manager

The Keysight License Manager utility is installed with the VSA software. The Keysight License Manager, along with the Keysight Software Manager website, enables you to easily manage the licenses for your VSA software. You can install licenses, transport licenses form one PC to another, and remove licenses that are no longer needed.

The Keysight License Manager displays the Host Name and Host ID. On an instrument, the Host IDs consist of an Keysight instrument model number and serial number. On a PC, the default model number is PCSERNO.

The Keysight License Manager can also be opened by clicking Start > (All) Programs > Keysight > Keysight License Manager or double clicking on the Keysight License Notifier icon in your Windows notification area.

Since the Keysight License Manager is a stand alone application, it has its own help system. For information on using the Keysight License Manager, click Help > Keysight License Manager Help from within the application or click Start > (All) Programs > Keysight > Keysight License Manager Help.

Keysight Software Manager Website

The Keysight Software Manager website is an Keysight website that is used to manage your 89600 VSA software licenses and subscriptions. Using the website you can:

To access the website, go to http://www.keysight.com/find/softwaremanager.

See Also

License Dialog Box

Status Tab