Transporting a License
The Transportable license is a license that can be moved from one PC to different PC. This allows you to use one license to run the 89600 Software on different PC's. However, only one PC at a time can use single license.
To transfer a license, an internet browser must be able to connect to the Keysight Software Manager website to transport a license. This connection takes a small, but noticeable, amount of time (up to 60–90 seconds) to complete a license transport operation.
Transporting a Transportable License Procedure
There are four steps required to transport a license (Deactivate, Synchronize, Assign and Install). See the Transport Licenses section of the Keysight Software Manager Utility Help for detailed instructions.
See Also