EVM Window Length (LTE-Advanced)
3GPP
3GPP, Custom: 1-512 samples
specifies the length of the window used for EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. calculations. The EVM window is centered in the cyclic prefix.
A value of will set according to the LTE Long Term Evolution standard for EVM measurements. Appendix F.5 of 3GPP TS Technical Specification 36.101 defines the window lengths for each bandwidth.
A EVM window length can also be specified in the range of 1-512 samples. A value of 512 samples corresponds to the entire CP 1) Contention period, or 2) Cyclic prefix length for Extended CP on a 20 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second. signal.
The standard states that the EVM for an LTE signal's subcarriers should be taken from the higher of the two EVM RMS averages calculated from the FFTs taken from the start and from the end of the EVM window. For example, an of 3 samples means that two FFTs would be taken. The starting points of the FFTs would be on the samples adjacent to the center sample of the CP. The EVMs for the subcarriers would come from the FFT Fast Fourier Transform: A mathematical operation performed on a time-domain signal to yield the individual spectral components that constitute the signal. See Spectrum. with the higher EVM RMS average. However, the location of the symbol FFT used for EVM calculations can be set specifically using the Symbol Timing Adjust parameter.
A value of 1 sample will cause the EVM to be measured from an FFT taken from the center of the cyclic prefix, since any further FFTs would have to be taken over the same sample points.
does not apply when Symbol Timing Adjust is set to or since these settings cause only one FFT to be taken starting from the specified location within the cyclic prefix regardless of the setting.
The selection of is not available for PRACH analysis since EVM window is not defined in the standard for PRACH Physical Random Access Channel.
See Also