Extended Freq Lock (LTE-Advanced)
Cleared
increases the range in which the demodulator will be able to lock onto component carrier x. Selecting this parameter will increase the frequency offset lock range from ±0.5x subcarrier spacing to ±2.5x subcarrier spacing on either side of the component carrier's center frequency. This increase in range causes the measurement to take longer so this parameter should be selected only when necessary.
See Also