LTE-Advanced Demod Properties Dialog Box

Menu Path: Analysis > LTE-Advanced Demod Properties

The LTE Long Term Evolution-Advanced Demod Properties dialog box contains parameters that let you configure the VSA to demodulate LTE-Advanced signals.

The LTE demodulator must be selected before this dialog box is available. To enable the demodulator, click Analysis > Measurement Type > Cellular > LTE-Advanced

The LTE-Advanced Demod Properties dialog box contains tab headings that group similar configuration parameters as follows:

See Also

Setting up an LTE-Advanced Measurement

Selecting LTE-Advanced Demodulation

Using a Standard Setup

Measurement Speed Considerations

Troubleshooting