Export CCx Settings to LTE Setup File... (LTE-Advanced)
allows you to export the configuration settings for the selected component carrier to a single LTE Long Term Evolution measurement setup file.
- In the , select the component carrier to configure.
- Click
- Navigate to the location where you want to save the single LTE measurement setup file (the default location is the LTE-Advanced sample signal folder, so you might want to choose the LTE folder instead).
- Enter a name for the new LTE setup file.
- Click
The configuration in the setup file will be used to configure the component carrier.
See Also