Import LTE Settings to CCx... (LTE-Advanced)
allows you to import LTE Long Term Evolution settings from a VSA setup file to configure a single component carrier (CCx, where x is the number of the component carrier).
- In the , select the component carrier to configure.
- Click
- Select a setup file that contains the configuration for a single LTE measurement.
- Click
The configuration in the setup file will be used to configure the component carrier.
See Also