Measurement Channel Selection Dialog (LTE-Advanced)
From this dialog, you can select which measurement channels are assigned to a component carrier. The LTE Long Term Evolution demodulator searches the selected measurement channels for the antenna port signals.
You can arbitrarily connect antenna signals to VSA measurement channels since the LTE demodulator autodetects the antenna ports by their reference signal patterns. However, certain traces are affected by the connection sequence since they refer to measurement channels (such as the MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. Info Table).
See Also