PUCCH Bits (LTE-Advanced)
specifies how much coding to undo before showing the bits from PUCCH Physical Uplink Control Channel on the Decoded Symbol Table. See 3GPP TS Technical Specification 36.212, Section 5.2.3 for a diagram of the coding operations performed on PUCCH.
The following is a list of the available PUCCH Bits selections and the resulting bits.
- - raw PUCCH bits are mapped to resource element locations and shown in the Symbol Table. No PUCCH bits are shown in the .
- - descrambled (channel coded) bits for each subframe are shown on the .
- - decoded bits for each subframe are shown in the .
For PUCCH Format 2/2a/2b, where both CQI Channel Quality Indicator / PMI Precoding Matrix Indicator and HARQ Hybrid Automatic Repeat Request-ACK Acknowledgement bits are jointly encoded, CQI / PMI information bits are listed first in a set of PUCCH bits, followed by HARQ-ACK information bits.
See Also