PUCCH Decode Parameters (LTE-Advanced)
The configure decoding of HARQ Hybrid Automatic Repeat Request-ACK Acknowledgement and CQI Channel Quality Indicator/PMI Precoding Matrix Indicator information bits. The parameter specifies the number of bits for all PUCCH Physical Uplink Control Channel transmissions for the selected uplink user allocation.
When the check box is selected for HARQ-ACK or CQI/PMI, the corresponding information bits will be decoded at the maximum length. The possible range of information bits is listed as follows:
- HARQ-ACK bits range: 0-21 bits
- CQI-PMI bits range: 0-11 bits
For best demodulation performance, specify HARQ-ACK and CQI/PMI manually.
See the PUCCH HARQ or CQI/PMI data results in the table for more information.
See Also