PUSCH Decode Parameters(LTE-Advanced)
The configure decoding of HARQ Hybrid Automatic Repeat Request-ACK Acknowledgement, RI, and CQI Channel Quality Indicator/PMI Precoding Matrix Indicator information bits.
See the PUSCH Physical Uplink Shared Channel HARQ, RI, and CQI/PMI data results in the table for more information.
Info Size parameter
The parameter specifies the number of bits for all PUSCH transmissions for the selected uplink user allocation.
When the check box is selected for HARQ-ACK, RI, or CQI/PMI, the corresponding information bit size will be autodetected as far as possible.
The possible range of information bits is listed as follows:
- HARQ-ACK bits range: 0-20 bits
- RI bits range: 0-15 bits
- CQI-PMI bits range: 0-144 bits
For best demodulation performance, specify manually.
Offset Index parameter
The parameter specifies the value of Ioffset for HARQ-ACK, RI, and CQI in the tables listed in 3GPP TS Technical Specification 36.213, Section 8.6.3.
The possible range of values are as follows:
- HARQ-ACK bits range: 0-15 bits
- RI bits range: 0-12 bits
- CQI-PMI bits range: 0-15 bits
See Also