Transmission Modes to Include in DCI Decoding (LTE-Advanced)
sets which Transmission Modes (1-9) are to be included in the detection of DCI Downlink Control Information Formats.
This property is useful in detecting the correct DCI Format. You can select multiple transmission modes, with the following exceptions:
- TM5 and TM6 cannot be included simultaneously, as simultanoeus detection of DCI Formats 1B and 1D is not possible
- TM3 and TM8 cannot be included simultaneously, as simultanoeus detection of DCI Formats 2A and 2B is not possible
- TM3 and TM9 cannot be included simultaneously, as simultanoeus detection of DCI Formats 2A and 2C is not possible
See Also