Uplink Bandwidth (LTE-Advanced)
The default value is the DL Down Link (forward link: from base station to cell phone) Analysis Bandwidth.
sets the uplink bandwidth (and total number of resource blocks) to be used in decoding certain DCI Downlink Control Information Formats. Below is a list of available bandwidths:
|
Available Bandwidths |
|---|
| 1.4 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second. (6 RB Resource Block) |
| 3 MHz (15 RB) |
| 5 MHz (25 RB) |
| 10 MHz (50 RB) |
| 15 MHz (75 RB) |
| 20 MHz (100 RB) |
See Also