CSI-RSPhase (LTE-Advanced)
shows the average phase error of the cell-specific reference signal for each CSI-RS Channel State Information Reference Signal/Rx path.
CSI channel state information-RSPhase is expressed in degrees relative to the CSI-RS phase error of the reference CSI-RS/Rx path and is calculated from the data in the Measurement Interval.
See Also