CSI-RSPwr (LTE-Advanced)
shows the average power of the cell-specific reference signal from a CSI-RS Channel State Information Reference Signal/Rx path.
RSPwr is expressed in dB relative to the power of CSI channel state information-RS on the reference CSI-RS/Rx path and is calculated from the data in the Measurement Interval.
See Also