Selecting LTE-A Test Models
To configure the VSA with E-UTRA Evolved Universal Terrestrial Radio Access Test Models on any number of component carriers, do the following:
- Put the VSA in LTE Long Term Evolution-A measurement extension.
- Set the appropriate number of component carriers and their frequency offsets from the center.
- On the tab of the dialog, click on and select an appropriate setup file from the %PROGRAMFILES%\Keysight\89600 Software <ReleaseVersion>\89600 VSA Software\Help\Signals\LTE-A\E-TM\CA 1) Channel Assignment or, 2) Carrier Aggregation for each CC.
See Also
Setting up an LTE-Advanced Measurement