Selecting LTE-Advanced Demodulation
Configures the 89600 VSA to demodulate LTE Long Term Evolution-Advanced signals (uplink and downlink) that are compliant with the 3GPP Technical Specifications listed in About Opts BHG and BHH: LTE-Advanced Modulation Analysis.
Configure the demodulator
After selecting the LTE-Advanced measurement type, you need to set certain configuration parameters on the tab of the LTE-Advanced Demod Properties dialog box to ensure demodulation of your signal. For a detailed setup procedure, see Setting up an LTE-Advanced Measurement.
Example recordings
The 89600 VSA includes several example LTE-Advanced signals that can be used to help you learn how to use the LTE demodulator. The included signals are listed in the Demo and Recorded Signals topic in the Getting Started book.
See Also