Antenna 3D Beam Pattern (LTE-Advanced)
The trace shows a three-dimensional representation of all available beam patterns in the system, including all layers, antenna groups, and UEs.
The Antenna 3D Beam Pattern trace is visible only when Antenna Array Shape is set to Rectangular
3D traces require a minimum OpenGL version of 2.1 to be enabled for proper three-dimensional rendering.
Data Settings
Data Settings allow you to adjust how data is transformed and presented in the trace. To adjust data settings, hover over the text in the upper left corner of the trace and click on the text.
Data settings are only available on the GUI, and are not configurable through the API 1) Access Preamble Indicator, or 2) Application Programming Interface.
Transform - Select the coordinate transform to be applied to the data before it is drawn.
- Log Magnitude: Specifies a logarithmic scale for the beam magnitudes. Magnitude is represented in dB, when Log Magnitude is selected.
- Linear Magnitude: Specifies a linear scale to be used for the beam magnitudes. Magnitude is represented in V, when Linear Magnitude is selected.
Magnitude Floor - The floor sets a minimum value to clip magnitude values to. The floor value is also used to set the origin of the polar plot. All values below the magnitude floor are clipped and set to the magnitude floor for displaying the data.
Opacity - Drag the slider to adjust the transparency of the drawn data. This can be useful to reveal data hidden by collisions.
See Also