Antenna Elevation Beam Pattern (LTE-Advanced)
The trace shows a two-dimensional representation of the elevation beam pattern on the specified layer index, for the specified antenna group at the azimuth angle specified by the 2D Beam Pattern Display Azimuth Angle setting (the data for the Elevation Beam Pattern trace is calculated by cutting the spherical surface with the specified azimuth angle).
The Antenna Elevation Beam Pattern trace is visible only when Antenna Array Shape is set to Rectangular
See Also