MIMO Eq Cond Number (LTE-Advanced)
shows the MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. condition number for each subcarrier.
See the MIMO Eq Cond Number trace topic in the 802.11n demodulator documentation for more information.
is only available when multiple measurement channels have been selected.
See Also