Exclude EVM Transient Time (LTE)
excludes the EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. results calculated from part of OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. symbols during a PUSCH Physical Uplink Shared Channel allocation change as specified by the standard in Section 6.5.2.1A of 3GPP TS Technical Specification 36.521-1.
See Also