LTE Demod Properties Dialog Box

Menu Path: Analysis > LTE Demod Properties

The LTE Demod Properties dialog box contains parameters that let you configure the VSA to demodulate LTE Long Term Evolution signals.

The LTE demodulator must be selected before this dialog box is available. To enable the demodulator, click Analysis > Measurement Type > Cellular > LTE

The LTE Demod Properties dialog box contains tab headings that group similar configuration parameters as follows:

See Also

Setting up an LTE Measurement

Selecting LTE Demodulation

Using a Standard Setup

Measurement Speed Considerations

Troubleshooting