Extended Freq Lock (LTE)
Cleared
increases the range in which the demodulator will be able to lock onto the signal. Selecting this parameter will increase the frequency offset lock range from ±0.5x subcarrier spacing to ±2.5x subcarrier spacing on either side of the center frequency. This increase in range causes the measurement to take longer so this parameter should be selected only when necessary.
See Also