Measurement Interval (LTE)

Default: 6 slots, 0 symbol-times

Measurement Interval determines how much data is sent to the demodulator and can be specified in slots plus symbol-times. The beginning of the measurement interval is specified as an offset from the Analysis Start Boundary. The offset is specified by the Measurement Offset parameter.

The Time Offset data result in the Error Summary trace shows the distance from the beginning of the Search Time trace to the beginning of the measurement interval.

See Also

Time Tab

Result Length

Measurement Offset

Search Time trace

Time trace