Time Offset (LTE)
is the offset to the Analysis Start Boundary and is expressed relative to the trigger t=0 point when Trigger Delay = 0 sec. When Trigger Delay is non-zero, then Trigger Delay will be subtracted from the Time Offset value.
The time offset will not exceed the analysis boundary period length (any integer multiple of the analysis boundary period will be subtracted from the TimeOffset).
See Also