Setting Up User Allocations (LTE)
For downlink autodetection, the demodulator can perform power-based autodetection or can decode PDCCH Physical Downlink Control Channel to determine user allocations. For uplink autodetection, the demodulator needs a unique slot to use for frame synchronization since there are no sync channels in uplink that are separate from the user channels. The sync slot can be autodetected or specified manually.
User channel allocations for uplink and downlink can also be defined manually.
For instructions on how to configure uplink or downlink channels and signals, click one of the links below:
See Also