RS-PRS (LTE)
The entry in the Error Summary table shows the current setting of the RS-PRS parameter on the Format tab of the dialog.
A value of means that the cell-specific reference signal's pseudorandom sequence is expected to follow the sequence defined by the standard for the current Cell ID setting.
A value of means that the RS-PRS is being autodetected.
See the RS-PRS measurement parameter topic for more information on RS-PRS.
See Also