Format Tab (LTE)
The tab of the LTE Demod Properties dialog box lets you configure parameters necessary for the VSA to demodulate the test signal.
Below is a list of the parameters in the tab:
- Duplex Mode
- TDD Time Division Duplex: A duplexing technique dividing a radio channel in time to allow downlink operation during part of the frame period and uplink operation in the remainder of the frame period.
- Direction
- Bandwidth
- Sync Type
- Cell ID
- RS-PRS
- Preset to Standard...
- Downlink Format Parameters
- Uplink Format Parameters
In downlink version of the , there is a diagram that shows the location of IQ Meas data points. This diagram is explained in the illustration below.
See Also