CP Length Mode (LTE)
indicates the CP 1) Contention period, or 2) Cyclic prefix length (Normal or Extended) that was autodetected by the demodulator or specified by the CP Length parameter. When the CP length is autodetected, the text "(auto)" will be displayed to the right of the value.
This metric only applies to the non-MBSFN region of the frame.
See the CP Length parameter for more information.
See Also