Available Summary Tables (LTE)
LTE Long Term Evolution modulation analysis provides the following summary tables:
- Beam Pattern Summary - shows 3D antenna beam pattern summary data for each beam in the signal.
- CCDF Summary - lists CCDF Complementary Cumulative Distribution Function power data.
- CW0/1 Decoded Symbol Table - shows the decoded bits from PBCH Physical Broadcast Channel, PCFICH Physical Control Format Indicator Channel, PDCCH Physical Downlink Control Channel, and PDSCH Physical Downlink Shared Channel.
- Decoded Symbol Table - shows the decoded bits from PUSCH Physical Uplink Shared Channel and PUCCH Physical Uplink Control Channel.
- DL Decode Info - shows the decoded data from PBCH, PCFICH, PDCCH, and PHICH Physical Hybrid ARQ Indicator Channel.
- Error Summary - provides information about the quality of the signal being analyzed.
- Frame Summary - provides EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format., power, modulation type, and number of resource blocks occupied for the channels and signals that are present.
- Symbol Table - shows the symbol values of the data subcarriers.
- MIMO Info Table - lists information about C-RS Cell-specific RS/Rx paths present in the signal. This information is calculated from the cell-specific reference signal.
- UE-specific RS Weights - lists the UE User Equipment (e.g. cell phone)-specific RS subcarriers and corresponding weights for each PDSCH allocation.
- UL Decode Info - shows the decoded control information from PUSCH and PUCCH.
See Also