Freq Err (LTE)
is the average frequency error of the data in the Measurement Interval and is specified as an offset from the current center frequency setting.
is calculated from the reference measurement channel for downlink signals.
See Also
is the average frequency error of the data in the Measurement Interval and is specified as an offset from the current center frequency setting.
is calculated from the reference measurement channel for downlink signals.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |