PUCCH DMRS (LTE)
PUCCH Physical Uplink Control Channel DMRS is the Demodulation Reference Signal for the uplink user's PUCCH channel. The modulation type used is QPSK Quadrature phase shift keying, but the constellation is rotated by a (Cyclic Shift). This is signified by "QPSK*" on the Frame Summary trace. PUCCH DMRS is transmitted on all subcarriers during the symbols specified by Table 5.5.2.2.2-1 in 3GPP TS Technical Specification 36.211.
When is selected, Frame Summary shows information about all detected PUCCH DMRS signals which match the PUCCH parameters in the LTE Allocation Editor. This information is located in the row for .
When is cleared, shows information about PUCCH DMRS in the row for the user currently selected for analysis and shows "---" for the other users' rows since the demodulator can only analyze one user at a time.
See Also