Error Vector Time (LTE)
shows the difference between the measured symbols and the reference symbols for each symbol in the Measurement Interval. The EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. values for subcarriers are plotted above their corresponding symbol-time on this trace. The values of the error vectors are usually plotted as a magnitude, but other formats can be chosen as well.
A marker placed on this trace which reads as follows
indicates that the marker is
- on symbol 80
- in the User03 channel allocation shown in the Composite Include list
- on subcarrier 103
- and has a value of ~0.33%, the RMS average error over all the subcarriers in this symbol being ~0.49% (see EVM for more information on how EVMs are calculated)
For uplink PRACH Physical Random Access Channel analysis, this trace's x-axis will be marked in subframes. The PRACH EVM data points are located at the subframe that the PRACH preamble begins in.
MBMS mixed-mode CP
MBMS Multimedia Broadcast Multicast Service signals are transmitted during the MBSFN region of MBSFN subframes using Extended CP 1) Contention period, or 2) Cyclic prefix mode (6 symbols per slot). The non-MBSFN region of these subframes (and the rest of the frame) can be transmitted in Normal or Extended CP mode.
For mixed-CP-mode LTE Long Term Evolution frames, traces that show time on the x-axis in units of syms (OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. symbols) would need unevenly spaced x-axis points to correctly represent the time locations of the symbols (since extended CP symbols are longer than normal CP symbols).
Instead of using non-uniform x-axis spacing of symbol points, the LTE demodulator shows the time axis as if all the slots used Normal CP (with 7 symbols per slot), and for MBSFN slots, the demodulator fills the first 6 symbols of the slot with the extended CP symbols, leaving the 7th symbol blank.
Downlink MIMO, Layers, and EVM Calculations
EVM values are calculated using physical channels' layer data. The LTE demodulator compares measured data (in IQ Meas) with the calculated ideal data (in IQ Ref) to compute an EVM. The data points for are always calculated and shown with precoding removed. For EVM calculations to work, data must also be shown with the precoding removed.
When the MIMO Decoding parameter is set to , data will be shown with the precoding present. This will cause EVM calculations to be invalid. For EVM calculations to be valid, must be set to
See Also