IQ Offset Per Slot (LTE)
shows the average IQ offset for each slot in the Measurement Interval. See the IQ Offset topic in the Error Summary book for more information about IQ offset calculation.
The trace is calculated and is valid for active slots only (slots that contain channel allocations, as defined in the LTE Allocation Editor or autodetected).
This trace is only available for uplink signals.
See Also