ChanEst Pwr - Band Packet Summary (MB-OFDM)
ChanEst Pwr (Channel Estimation Power) is the absolute power in the Channel Estimation section (6 symbols) of the preamble in the current MB-OFDM Packet for each Band (Low, Mid, and High) averaged over each of the three bands individually and computed in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer.
See Also
Band Packet Summary Table (MB-OFDM)