Header EVM - Band Packet Summary (MB-OFDM)
Header EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. (Error Vector Magnitude) is the RMS level of the Error Vector Magnitude in the Header section of the current MB-OFDM Packet averaged over each Band (Low, Mid, and High) individually. It is displayed in dB and as a percentage (%rms) for each of the bands.
See Also
Available Band Packet Summary Data (MB-OFDM)
Available Packet Summary Data (MB-OFDM)