Hdr Pwr - Band Packet Summary (MB-OFDM)
Header Power is the absolute power in the Header section of each Band (Low, Mid, and High) in the current MB-OFDM Packet averaged over each of the three bands individually and computed in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer.
See Also
Band Packet Summary Table (MB-OFDM)