Overall EVM - Band Packet Summary (MB-OFDM)
Overall EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. (Error Vector Magnitude) is the RMS level of the Error Vector Magnitude for each Band (Low, Mid, and High) in the header and the payload of the current MB-OFDM Packet averaged over each band individually. It is displayed in dB and as a percentage(%rms) for each of the bands.
See Also
Band Packet Summary Table (MB-OFDM)