Packet Pwr - Band Packet Summary (MB-OFDM)
Packet Power is the absolute power in each Band (Low, Mid, High) of the current MB-OFDM Packet averaged over each of the three bands individually and computed in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer.
See Also
Band Packet Summary Table (MB-OFDM)