Pyld Pwr - Band Packet Summary (MB-OFDM)
Payload Power is the absolute power in the Payload (PSDU 1) PHY Service Data Unit, or 2) PLCP SDU) section of the current MB-OFDM Packet for each Band (Low, Mid, and High) averaged each band individually and computed in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer.
See Also
Band Packet Summary Table (MB-OFDM)