Rel CE Pwr - Band Packet Summary (MB-OFDM)
Rel CE Pwr (Channel Estimation Power) is the power in the Channel Estimation (6 symbols) section of the preamble for each Band (Low, Mid, and High) in the MB-OFDM Packet relative to Sync Power for that band as specified in the standard. (See About Opt BHB: Multiband-OFDM.).
See Also
Band Packet Summary Table (MB-OFDM)