Rel Pyld Pwr - Band Packet Summary (MB-OFDM)
Rel Pyld Pwr (Payload Power) is the power in the Payload (PSDU 1) PHY Service Data Unit, or 2) PLCP SDU) section of the MB-OFDM Packet for each Band (Low, Mid, and High) relative to Sync Power for that band as specified in the standard. (See About Opt BHB: Multiband-OFDM.).
See Also
Band Packet Summary Table (MB-OFDM)