Det Pmbl Type (MB-OFDM)
If the Preamble Type is set to , Det Pmbl Type displays the detected preamble type for the current measurement; otherwise Det Pmbl Type displays the current setting.
See Also
If the Preamble Type is set to , Det Pmbl Type displays the detected preamble type for the current measurement; otherwise Det Pmbl Type displays the current setting.
See Also
Copyright © 2000-2024 Keysight Technologies, Inc. |