EVM Pk (MB-OFDM)
Menu Path:
EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. Pk (Error Vector Magnitude Peak) is the highest EVM value of all the data and pilot subcarriers EVMs in the . The output provides both the percentage EVM (%) and the number of the symbol where the peak EVM occurred.
See Also