IQ Offset (MB-OFDM)
Menu Path:
IQ Offset (also called I/Q origin offset or carrier leakage) indicates the magnitude of the carrier feedthrough signal as measured during the channel estimation sequence portion of the preamble. When there is no carrier feedthrough, IQ offset is zero (minus infinity dB).
IQ Offset is the same as IQ Offset for Digital Demodulation. For more information about this parameter, see IQ Offset (Digital Demod).
See Also