SyncCorr Min (MB-OFDM)
SyncCorr Min (Synchronization Correlation Minimum) gives the minimum correlation between the measured Packet/Frame Synchronization sequence portion of the Preamble and the ideal Packet/Frame Synchronization sequence. The SyncCorr (Synchronization Correlation) is computed on a symbol by symbol basis so the SyncCorr Min is the lowest of these individual symbol correlations. The result shows both the value at this symbol expressed in percentage and the location of the symbol. A value of 100% indicates perfect correlation and a value of 0 indicates no correlation.
See Also
CError Summary Table (MB-OFDM)