Packet Summary Table
The Packet Summary table provides measurement and analysis information unique to the MB-OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Packet Summary trace data and MB-OFDM modulation analysis. The Packet Summary Table displays results for all bands (when hopped). Results per band are available in the Band Packet Summary Table.
The MB-OFDM Packet consists of the following: Preamble (Packet/Frame Sync and Channel Estimation), Header, and Payload. A list of the available packet data is provided in the Available Data Results topic, which also links to detailed descriptions for each packet result.
See Also