Payload EVM - Packet Summary (MB-OFDM)
Payload EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. (Error Vector Magnitude) is the RMS level of the Error Vector Magnitude in the Payload (PSDU 1) PHY Service Data Unit, or 2) PLCP SDU) section of the current MB-OFDM Packet averaged over all bands as specified in the standard. (See About Opt BHB: Multiband-OFDM.) It is computed in %rms.
See Also
Payload EVM - Band Packet Summary Table (MB-OFDM)