Sync Pwr - Packet Summary (MB-OFDM)
Synchronization Power is the absolute power in the Packet/Frame Sync section of the current MB-OFDM Packet preamble averaged over all bands and computed in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer. Sync Power is the reference for the relative power values.
See Also
Sync Pwr - Band Packet Summary Table (MB-OFDM)