Eq Impulse Response (Low | Mid | High Band) (MB-OFDM)
The Low | Mid | High Band (Equalizer Impulse Response) trace shows the impulse response for the corresponding Low | Mid | High Band of the equalization filter. The is computed using both the Channel Estimation Sequence portion of the preamble and the data symbols. To see a trace with all Low, Mid, and High Bands combined, see Composite Eq Impulse Response.
The per band results are computed when performing TFI/TFI2 analysis when Frequency Hopping Analysis is NOT set to Force FFI.
The result length will be four times the FFT Fast Fourier Transform: A mathematical operation performed on a time-domain signal to yield the individual spectral components that constitute the signal. See Spectrum. length so a total of 512 points.
This is similar to, but not the same as, the Digital Demod . The differences are:
- computes this by comparing the and data, while demodulation computes it from the preamble/data of the burst.
- typically uses a running average to average multiple scans when computing the . demodulation does not average, but computes a new equalizer response for each burst.
- The equalization filter is inherent to demodulation, it cannot be enabled/disabled like .
See Also